Browse FAQs

Can I connect the condenser ducts of an ACSC1XX unit directly outside?

Published date: 17 July 2020


Issue:
This document explains if you can connect the condenser ducts directly outside?

Product line:
ACSC1XX.

Environment:  
All Serial Numbers.
 
Cause:  
FAQ.

Resolution:
Yes, with certain exceptions. The SC condenser cannot tolerate inlet air below 32 F (0 C), so the unit will have problems during the winter in many parts of the world. Also, the condenser cannot tolerate inlet air hotter than 105 F (40 C). It may be easier to only exhaust the hot air outside and draw the condenser inlet air from the room. Contact your Config Team rep or Systems Engineer for additional assistance.
 
 
 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.