Browse FAQs

The NetShelter CX doors are not aligned. Can they be adjusted?

Published date: 30 May 2019

Issue:
NetShelter CX Door Misalignment

Product Line:
NetShelter CX
 
Environment:
All versions and serial ranges.
 
Cause:
The cause for an uneven door may not be known but it can be corrected.
 
Resolution:
Make sure the floor is even and, if not, adjust the leveling feet and level the cabinet.  
Also, the doors may move slightly in transit. If this happens the hinges can easily be adjusted to fix this. Use a phillips head screwdriver to move the hinge as required.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.