Browse FAQs

Whether to install a suction line drier or liquid line drier

Published date: 18 July 2020

Issue:

Whether to install a suction line drier or liquid line drier

 

Product line:

All Air Cooled Units

 

Environment:

All Product models, all serial numbers

 

Cause:

Remove contaminants from system

 

Resolution:

Installing a suction line drier in an ACRP DX is a tight fit, but possible.  The obvious benefit of a suction line filter drier is the added protection given the system if a burnout should occur. The filter will effectively prevent contamination resulting from the failure from traveling back through the suction line into the other parts of the system. This will minimize the contamination remaining in the system when the inoperative compressor is removed.  With this said, it is preferred to put the drier in the suction line.  If a technician cannot find a suitable suction line drier with replaceable cores to fit inside the ACRP, a liquid line drier would be fine.  It is ok to use an additional liquid line drier with replaceable cores.  This can be handy since a technician will have more room on the outside liquid line to install isolation valves to keep the downtime to a minimum when replacing cores.  The ACRP uses Danfoss liquid line drier pn # 023Z4581, 5/8" ODF SOLDER. You will need to find a small suction line filter drier.  

 

It is imperative for the technician to allow a minimum of 48 hours of unit operation before the liquid line filter-drier or the suction line filter-drier. After the cleaning procedure is completed, recheck in approximately one to two weeks to ensure that the system condition and operation is completely satisfactory.

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.