{}

Nos marques

Consulter notre FAQ

How tall is the NetShelter WX with the optional castor kit attached?

Issue:
Customers may ask for the total height of the NetShelter WX with the optional castor kit attached.

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
Cabinets that are floor mounted may have height restrictions.

Resolution:
The NetShelter WX with the optional castor kit attached is approximately 731 mm (28.78") tall.

APC {country}