{}

Nos marques

Consulter notre FAQ

NetBotz 300-500 Series | Downloading and Installing the Advanced View Management Software

Issue:
Where to download and how to install the NetBotz Advanced View software application.

Product line:
NetBotz 300-500 Series [v3 Hardware] (355, 455, 450, 550, & 570)

Environment:
NetBotz v3 Hardware (all versions)
Advanced View Software Application

Cause:
NetBotz 300-500 series appliances can only be configured using the Advanced View software application.

Resolution:

Advanced View can be found on the CD that was shipped with the Appliance.  Insert the CD into your computer and install the Advanced View software using the provided executable file on the CD.

NOTE: It is recommended that you match the version of Advanced View with the version of Botzware on the appliance. Failure to do so may cause unsuspected results and errors.
Downloading Advanced View from the Web for Models: 355, 455, 450, 550, & 570

1) Navigate to: http://updates.apc.com/botz/av/install.htm

2) Download the Installer for your OS.

3) Follow the instructions on the download page to begin installation.

4) Follow the prompts to complete the installation.
NOTE: The installation also includes a utility for configuring the network settings of an appliance.  You can exit out of this if it is not needed.

5) Launch the Advanced View software from the start menu or the Desktop Icon.

Note: NetBotz | End of Sale & End of Support Information

APC {country}