{}

Nos marques

Consulter notre FAQ

Does the AR2144BLK or AR2145BLK NetShelter VX Seismic have leveling feet or castors available as an accessory?

Issue:
A customer may ask if castors are an accessory for our NetShelter VX cabinet.

Product Line:
NetShelter VX

Environment:
All versions and serial ranges.

Cause:
Castors can be used to move the cabinet much eaqsier.

Resolution :

The NetShelter VX cabinets do not offer castors as an accessory. These cabinets are approved for NEBS GR-63-CORE seismic installation, which does not include the use of castors.
Also see attached document.

APC {country}

Pièce(s) jointe(s)

AR2144BLK AR2145BLK Feet and Castors.docAR2144BLK AR2145BLK Feet and Castors.doc [102 KB]