Browse FAQs

Cannot Launch to Private Devices from StruxureWare Data Center Expert UI Installed on Linux

Published date: 20 July 2020

 

Issue
The StruxureWare Data Center Expert client cannot launch to devices on the private LAN when it is installed on Linux with the network proxy configured.

Product Line
StruxureWare Data Center Expert

Environment
StruxureWare Data Center Expert user interface (any version)
Linux

Cause
Linux private device launch does not work if the DCE Linux Client has a network proxy enabled.

Resolution
Add the DCE server IP address to the Linux client network proxy ignore list, or disable the proxy.

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.