Browse FAQs

Why does the Windows Service for PowerChute Business Edition Agent not start with System log error 7024?

Published date: 17 March 2021

Issue:
Windows Service for PowerChute Business Edition Agent does not start.

Two ways of checking this:

* A dialog pop-up message is shown after the service fails to start

* The Windows Event Log shows:

(1) Windows Application log
Source: APC PBEAgent
Type: Error
Event ID: 101
Description: Error: 0, Time out 90 seconds. Service start operation canceled.

(2) Windows System log
Source: Service Control Manager
Type: Error
Event ID: 7024
Description:APC PBE Agent terminated with the following error: 0(0x0)

Product Line:
PowerChute Business Edition (PCBE)

Environment:
All Windows OS

Cause:
1 - This can be caused by a large number of temporary files in the \temp folder (usually C:\Windows\temp).
2 - Corrupt or missing m11.cfg file. 

Solution:
1 - Delete the temporary files in the \temp folder.
2 - For corrupt or missing m11.cfg file, uninstall and reinstall the PowerChute Agent. 


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.