Browse FAQs

Data Center Expert | Deleting a device causes all associated information to be deleted.

Published date: 22 July 2020

Issue:
Deleting a device from StruxureWare Data Center Expert causes all associated sensors and historical data to be deleted.

Product Line:
NetBotz Central (NBC)
InfraStruXure Central (ISXC)
StruxureWare Central (SWC)
StruxureWare Data Center Expert (DCE)
NetBotz Appliances (NB)
Network Management Cards / 3rd party devices

Environment:
NBC, ISXC, SWC, & DCE (all versions)
NetBotz Appliances
SNMP Devices
Modbus TCP/IP Devices

Cause:
When a device (NetBotz, SNMP, Modbus TCP/IP) is deleted all associated information for the device is purged from the server's database. This means that all historical sensor data, alert data, and surveillance data will be deleted.

Resolution:

If historical data must be kept for a device the device CAN NOT be removed from the software.  Once the device is deleted the sensors and historical data are also removed.  There is no workaround at this time.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.