Galaxy VX; How to configure the Network Communications options
Published date:
15 July 2020
Issue:
How to configure the Network Communications options for Galaxy VX
Product line: Galaxy VX - all
Environment: All
Cause: How to set up network communications for the UPS
Resolution: The network can be configured for the display and for the cards in Smart Slot 1 and Smart Slot 2.
From the home screen on the display select Configuration > Network and select either Display, Smart Slot 1, or Smart Slot 2 if present.
Configure the following settings: TCP/IPv4: Enable IPv4 (if applicable), and select the Address Mode (Manual, DCHP, or BOOTP).
TCP/IPv6: Enable IPv6 (if applicable), select Auto Configuration or Manual Configuration, and select the DHCPv6 Mode (Router controlled, Non-Address Information Only, Never, or Address and Other Information).
NOTE: Tap Addresses to see all valid IPv6 addresses.
Web Access: Enable Web (if applicable) and select the Access Mode (HTTP or HTTPS). NOTE: Not available for Smart Slots.
FTP server: Enable FTP (if applicable). NOTE: Not available for Smart Slots.
When all settings have been completed, tap OK to confirm your settings.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.