Smart-UPS VT-G3500; Load does not turn on automatically after an outage/shutdown
Published date:
10 July 2019
Issue:
Load does not turn on automatically after an outage/shutdown
Product line:
Smart-UPS VT-Galaxy 3500
Environment:
All Product models, all serial numbers
Cause:
The system is set to not auto start by default
Resolution:
You can set the load to turn on automatically after an outage from the PowerView display.
1. Go to Setup menu
2: Select System
3: Select Auto Start
4. Change value to On
This may take one reboot of the UPS to take affect, and you will need to turn on the load manually then. After that first reboot it should automatically turn on in the future.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.