Which SmartSlot accessories are supported by the Galaxy 3500 (g3500) UPS?
... supported by the Galaxy 3500 (g3500) UPS ? ... Facility 3 Phase UPS MGE Galaxy 3500 models ... supported by the Galaxy 3500 UPS (g3500) ... ... with the g3500 UPS . ... with the g3500 UPS . ... inputs, ( 1 ) output per ... ... in the g3500 UPS . ... in the g3500 UPS . ... front panel/ UPS door will not ... 1 .) Purchase ... ... an APC ap9600 single slot SmartSlot expansion ... ... top of the UPS . ... SmartSlot in the UPS frame. ... comes with a 10 ' cable. ... communication cable can be routed so that the chassis can sit on top of the UPS .