Configuring the Native Serial Shutdown Support in Windows 2000, XP, or 2003
... not supported with Smart - UPS model family SMT ... Connect the UPS to the PC ... ... Click on the UPS tab to configure ... serially with a UPS . If the UPS tab is not ... ... reboot, the UPS tab will be ... ... Note: The UPS tab is NOT ... configure an APC USB UPS and will not ... if an APC USB UPS is attached to ... The UPS service is currently ... The UPS service, by ... ... configured, the UPS service will start ... ... and finally a UPS model family. Once the UPS has been selected ... ... and start the UPS service, click ...