Search FAQs
BMS AP9921X-AP9922; alarms “Battery High Chemistry Voltage”
Issue:
BMS AP9921X-AP9922; alarms “Battery High Chemistry Voltage”
Product line:
Battery Management System (BMS) AP9921X & AP9922
Environment:
All models, all serial numbers
Cause:
The voltage of a battery is above the threshold for the battery type.
Resolution:
If a specific battery causes repeated alarms (especially if the voltage continues to increase), the battery is failing. Replace the battery.
Released for:APC United Arab Emirates
Did this answer your question?
Explore more
Range:
Explore more
Range: