Search FAQs
Can you change the cycle time on an InRow ACRD?
Issue:
Can you change the cycle time on an InRow ACRD?
Product line:
InRow DX
Environment:
Data Center Cooling
Cause:
Resolution:
The unit cannot operate in Lead/Lag mode under InRow operations. You will have to select HACS,RACS or Spot allowing you to access operational screen to configure Lead/Lag.
Runtime balancing can be enabled through the following path: Configure Group->Runtm Bal. When enabled the controls will shuffle primary and backup roles of units periodically to balance the system run-time of the units in the group.
Runtime balance is 72 hours. Please note that this does not mean that the units will switch every 72 hours. This means that the units will switch when there is 72 hours of runtime difference between the units.This is not changeable.
Can you change the cycle time on an InRow ACRD?
Product line:
InRow DX
Environment:
Data Center Cooling
Cause:
Resolution:
The unit cannot operate in Lead/Lag mode under InRow operations. You will have to select HACS,RACS or Spot allowing you to access operational screen to configure Lead/Lag.
Runtime balancing can be enabled through the following path: Configure Group->Runtm Bal. When enabled the controls will shuffle primary and backup roles of units periodically to balance the system run-time of the units in the group.
Runtime balance is 72 hours. Please note that this does not mean that the units will switch every 72 hours. This means that the units will switch when there is 72 hours of runtime difference between the units.This is not changeable.
Released for:APC United Arab Emirates
Explore more