Technical FAQs

Ask a Question

Which External Battery Pack (XLBP) and RBC is compatible with my Smart-UPS On-Line (SRT) model?


Issue:

Which External Battery Pack (XLBP) and RBC is compatible with my Smart-UPS On-Line (SRT) model?

Product Line:

Smart-UPS Online

Environment:

All SRT models and all SRT external battery packs, All Serial Numbers

Cause:

There are specific External Battery Pack and RBC models which are compatible with a group of UPS models.

Resolution:

When selecting an External Battery Pack (XLBP) or RBC for a UPS system, use the table below to select compatible models.

NOTE: Each external battery pack has a keyed mating connector that is only compatible with its corresponding UPS. If you find that a connector is binding or requires excessive force to insert you should STOP and check compatibility of the UPS and battery pack. 
 
UPS Model (beginning with) Battery Type Replacement Battery Pack (RBC) Battery Module Voltage Total Battery Voltage for the UPS External Battery Pack Connector Color External Battery Pack (XLBP)
SRT1000XL, SRT1500XL, SRT1000RMXL, SRT1500RMXL Maintenance-free sealed Lead-Acid battery with suspended electrolyte : leakproof APCRBC155 48 VDC 48 VDC Blue SRT48BP
SRT48RMBP
SRT1000UXI-LI, SRT1500UXI-LI Lithium Ion NMC chemistry No internal battery - uses external battery system NA See manual Blue XBP48RM1U-LI
Note: The UPS does not
support any other make/type of battery packs.
SRT2200XL, SRT2200RMXL Maintenance-free sealed Lead-Acid battery with suspended electrolyte : leakproof APCRBC141 72 VDC 72 VDC Green SRT72BP
SRT72RMBP
SRT3000XL, SRT3000RMXL Maintenance-free sealed Lead-Acid battery with suspended electrolyte : leakproof APCRBC152 96 VDC 96 VDC Brown SRT96BP
SRT96RMBP
SRT5K, SRT6K Maintenance-free sealed Lead-Acid battery with suspended electrolyte : leakproof APCRBC140 96 VDC 192 VDC White SRT192BP
SRT192RMBP
SRT8K, SRT10K Maintenance-free sealed Lead-Acid battery with suspended electrolyte : leakproof APCRBC140 96 VDC +192 VDC
-192 VDC
White SRT192BP2
SRT192RMBP2


 
Was this helpful?
What can we do to improve the information ?