Technical FAQs

Ask a Question

Video: How to configure the display network settings on a Galaxy VM

Issue:
Configuring Network Settings on Galaxy VM UPS Display
 
Product line:
Galaxy VM
 
Environment:
All Product models, all serial numbers
 
Cause:
How to configure the display network settings on a Galaxy VM

Resolution:
Go over the steps required to configure the network settings on a Galaxy VM.
 
The Galaxy VM comes equipped with a built-in network management card with the display, and has 2 empty SmartSlots for additional NMC if desired.  The Galaxy VM supports the AP9630, AP9631 and AP9635 SmartSlot cards only. 
 
Start at the Home screen.
Select 'Configuration'

From the Configuration screen select 'Network' then 'Display' Make the changes needed to configure the network settings for the display.

The following video demonstrates this procedure:

Was this helpful?
What can we do to improve the information ?