What is the flow rate required for the InRow ACRD20x fluid-cooled unit?
Issue:
What is the flow rate required for the InRow ACRD20x fluid-cooled unit?
Product line:
ACRD200, ACRD201
Environment:
Data Center Cooling
Cause:
Resolution:
Each InRow ACRD20x fluid-cooled unit requires a flow rate of 10gpm within its loop. This is for a single ACRD20x piped to a single outdoor fluid cooler. The flow rates will vary for custom configurations consisting of multiple ACRD20x units to a single outdoor dry-cooler. Additional guidance on flow rates can be obtained from the Applications Engineering team.