Technical FAQs

Ask a Question

What color is the NetShelter paint?

Issue:
Customers may ask for the paint color of the NetShelter cabinet.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Customers may want to repair or match paint.

Resolution:
The NetShelter cabinets colors are as follows:
Black = RAL 9005, Textured.
White = RAL 9003 Fine Textured.
Gray = RAL 7035 Textured.
If you have further questions please contact Technical Support.
Was this helpful?
What can we do to improve the information ?