Are APC Cat 6 Patch Panels color coded for 568B or 568A?
Issue: The installer needs to know the color code on the rear of the Cat 6 patch panel.
Product Line: Cables and Connectivity Solutions, Patch Panels
Environment: CAT6PNL-24, CAT6PNL-48
Cause: Installers need to know if the patch panel has the color code they require.
Resolution : see below
The CAT6PNL-xx series of Patch Panels have both 568B and 568A color codes. Cat 5e, 6 and 6a patch cables and other cabling accessories can be viewed at www.apccables.com