Technical FAQs

Ask a Question

Fiber Pod Extender Signal Quality Variance

Issue:

Fiber Pod Extender Signal Quality Variance

Product Line:

NetBotz

Environment:

NetBotz Fiber pod extender NBAC0212

Cause:

NetBotz can still communicate with pods even with some signal loss.

Resolution:

The NetBotz Fiber Pod Extenders will function properly with up to 10dB level of signal loss between the local and remote units of the extender.
Was this helpful?
What can we do to improve the information ?