Technical FAQs

Ask a Question

NetBotz Appliances version 1 and 2 Operating Environments

Issue:

NetBotz version 1 and 2 Appliances Operating Environments

Product Line:

NetBotz

Environment:

NetBotz version 1 and 2

Cause:

Opearting environment

Resolution:

The NetBotz Appliances and pods are designed for indoor use only.

The environmental operating conditions are as follows:

* Temperature: 35F to 120F (1.6C to 48.8C)
* Humidity: 10% to 90% non-condensing 
Was this helpful?
What can we do to improve the information ?