Technical FAQs

Ask a Question

ISX Central | Enabling or disabling the private LAN will cause a new self signed SSL certificate to be generated.

Issue:
Enabling or disabling ISX Central Private LAN will cause the server to generate a new self signed SSL certificate

Product Line:
InfraStruxure Central (ISXC)

Environment:
InfraStruxure Central (Prior to 6.2)

Cause:
When working with SSL certs, you will need to re-add the cert if you enable or disable DHCP on the private LAN or if you change IP information on the private LAN. This is a known issue.

Resolution:

This issue was resolved in InfraStruxure Central 6.2
 
Was this helpful?
What can we do to improve the information ?