Technical FAQs

Ask a Question

What is the ACRC Cable Length?

The cable lengths are based on UL electrical standards for that type of device. Per UL the maximum cable length can not exceed 6' and must be at least 2'.
Was this helpful?
What can we do to improve the information ?