Technical FAQs
Technical FAQs
One note is that environmental monitoring events can trigger a shutdown of the PowerChute Network Shutdown client and the UPS. However, a clearing of the Environmental condition will not cause the UPS or the server to turn back on. The user must turn the UPS back on if a shutdown is initiated by PowerChute. When a UPS switches to battery and is eventually shutdown by PowerChute, it can be configured to turn back on once power is restored.
Note: Depending on the UPS application running on the AP9635/AP935CH, only temperature and/or humidity violations may be supported strictly for monitoring purposes, no PowerChute Network client shutdown operations. For example, the sypx application does support PCNS client shutdown based on environmental events assuming the UPS is online but other AP9635/AP9635CH applications do not necessarily support them.