Technical FAQs

Ask a Question

Video: Changing the display Language, Date Format & Temperature Units on a Galaxy VM

Issue:
Configuring Display Language, Date & Temperature Units on Galaxy VM UPS
 
Product line:
Galaxy VM
 
Environment:
All Product models, all serial numbers
 
Cause:
Depending on application, the UPS display may need to be adjusted to conform to local language and formatting.

Resolution:
Go through the steps to change the display settings on a Galaxy VM.
 
Start from the Home screen
Select ‘Configuration’
Select ‘Display’
Select ‘Preferences”

Change the language to your desired language

The following video demonstrates this procedure:
 
Was this helpful?
What can we do to improve the information ?