Technical FAQs

Ask a Question

Video: How to run PowerChute Network Shutdown setup wizard & configure for VMware ESXi hosts and vCenter Server

Issue:
Need to setup PowerChute Network Shutdown for VMware ESXi hosts and vCenter Server.

Product:
PowerChute Network Shutdown v4.2

Environment:
VMware ESXi 5.x and 6.x hosts and VMware vCenter Server 5.x and 6.x

Solution:



Review PowerChute Network Shutdown Installation Guide http://www.apcmedia.com/salestools/PMAR-9HBK44/PMAR-9HBK44_R4_EN.pdf?sdirect=true

The PowerChute Network Shutdown VMware User's Guide http://www.apcmedia.com/salestools/PMAR-9DNLQK/PMAR-9DNLQK_R3_EN.pdf

and Application Note 180 http://www.apcmedia.com/salestools/SJHN-92FLU8/SJHN-92FLU8_R6_EN.pdf?sdirect=true

NOTE:
For help deploying the PowerChute Appliace on VMware see FAQ FA296461.
For assistance installing PowerChute Network Shutdown on Windows OS see FAQ FA250921
For assistance installing PowerChute Network Shutdown on VMware vMA see FAQ FA313604
Was this helpful?
What can we do to improve the information ?