Technical FAQs

Ask a Question

NetBotz v3 | How do I configure location settings?

‚ÄčIssue:
Process for configuring location settings on v3 NetBotz Appliances.

Product Line:
NetBotz v3 (355, 455, 450, 550, & 570)

Environment:
NetBotz v3 (all versions)

Resolution:

1) Log into your NetBotz Appliance as an administrator using the Advanced View application.

2) Select the Configuration Tab and then under Appliance Settings select Location.

3) Enter in the Values for the different location fields that you would like to define.
NOTE: StruxureWare Data Center Expert will only pull in the main location field to display.

4) Use the Pods/Sensors navigation tree to navigate into the different PODs and sensors that are attached to the NetBotz Appliance.  Each POD and sensor can have its Location Data Values defined.
NOTE: StruxureWare Data Center Expert will only pull in the main location field of the Sensor Pods, Rack Access Pods, and wireless devices to display.

5) Click OK to save the changes.
Was this helpful?
What can we do to improve the information ?