Technical FAQs

Ask a Question

Can a NetBotz configuration backup be used on another NetBotz appliance?

Issue:
Using a NetBotz configuration backup on a different NetBotz appliance does not configure both units identically.

Product Line:
NetBotz

Environment:
NetBotz backup / restore on any version

Cause:
Due to differences in NetBotz Pod and sensor IDs from one appliance to another, importing a backup from one appliance to another will not import all configuration options.

Resolution:
The backup and restore functionality is meant to back up a single NetBotz appliance and restore that same appliance to a known good state should something happen with the appliance configuration. If you do restore to a different appliance, some settings such as alert actions or user login information will get transferred to the new appliance but any configuration for thresholds or pods or sensors will look like unplugged sensors and pods sue to the difference in pod and sensor IDs. It is recommended that you do not use this functionality between different appliances.
 
Was this helpful?
What can we do to improve the information ?