Technical FAQs

Ask a Question

How many InRow units can be grouped together at one time?

Issue:
How many InRow units can be grouped together at one time?

Product Line:
All InRow units ACRCXXX, ACRPXXX, ACRDXXX, ACSCXXX

Environment:
All serial numbers.

Cause:
Installation

Resolution:
The maximum amount of units that can be in a group are 12. This applies to all InRow units designated above.
Was this helpful?
What can we do to improve the information ?