Technical FAQs

Ask a Question

Why do device menus not display as expected when launched from StruxureWare Data Center Expert?


When the device user interface is launched from StruxureWare Data Center Expert, menus in the device UI are not displayed as expected

Product Line:
StruxureWare Data Center Expert


Microsoft Internet Explorer 6
StruxureWare Data Center Expert version 7.x


This issue is known to occur when IE6 is set as the default browser. StruxureWare Data Center Expert does not support IE 6. Although IE 7 is not known to exhibit display issues, it is no longer supported.


Upgrade the default browser on your computer. Supported browsers are:
• Microsoft Internet Explorer® 8, 9, 10
• Mozilla® Firefox® 17.0
• Google Chrome™ 23.0
Was this helpful?
What can we do to improve the information ?