Technical FAQs

Ask a Question

How to remove ceiling panels to access cabling on an EcoAisle


Issue:
How to remove ceiling panels to access cabling on an EcoAisle

Product line: 
EcoAisle

Environment:  
Only ACRC100, EcoBreeze, ACRC301X

Cause:  
Install

Resolution:

•         Over aisle access

•         A customer still needs to access the cabling on top of the racks.  This system is designed with the user in mind.  Access to the top of the racks is done with out the use of tools.  On a ceiling system it is as easy as removing a drop ceiling tile with a lift, angle and drop.  The duct system has an air-block system that can be removed with a thumbscrew.

 

 

 

 

 

 

 

 

 

 

 

Was this helpful?
What can we do to improve the information ?