ZAMBIA - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Modular Access Floor
Uniflair Technical Floor
Uniflair Office Floor
Uniflair Building Floor
Air Economizers
Ecoflair Air Economizers
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
Static Transfer Switches
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
Module Optimized Cooling
Chilled Water System
Power Modules
Enclosed Power Module
Skid Mounted Power Module
IT Modules
SmartShelter Container
SmartShelter Module
SmartShelter Data Hall
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
Data Center Assessment Services
Install
Installation Services
Operate
Battery Replacement Services
Extended Warranties
Preventive Maintenance
Service Plans
Optimize
Training Services
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
ZAMBIA - Choose Country or Region
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
Error When Attempting a Runtime Calibration in PowerChute Business Edition
Issue:
Error When Attempting a Runtime Calibration in PowerChute Business Edition
Product Line:
PowerChute Business Edition
Environment:
All supported OS
Cause:
1) The battery has less than 100% charge:
2) The load on the UPS is 10% or less:
Resolution:
Two conditions need to be met in order to perform a calibration:
1) The battery charge needs to be at 100%,
2) The load on the UPS needs to be greater than 10% of the battery capacity