Technical FAQs

Ask a Question

Events which trigger Messages and E-mails in PowerChute Business Edition.

Issue:
What events trigger an e-mail message in PowerChute Business Edition?

Product:
PowerChute Business Edition version 9.0 and above

Environment:
All support OS

Solution:

Attached is a list of events that will trigger an E-mail or Message depending on whether you configured for E-mail or Messaging*. Some of these events cannot be un-configured when using the Server portion of PowerChute Business Edition. This list may change in future releases of PowerChute Business Edition depending on software, UPS, and accessory capabilities.

This list is available in PowerChute Help!

*NOTE: Messaging is only available on Windows XP, 2003

Was this helpful?
What can we do to improve the information ?