Technical FAQs

Ask a Question

Does APC manufacture a Cat 5E rated RJ45F/RJ45F inline coupler?

Issue:
Many couplers are not rated for high speed networking. 
 
Product Line:
Cables and Connectivity Solutions, inline couplers
 
Environment:
All versions and serial ranges
 
Cause:
Customers need to connect patch cables together to extend the length of high speed network cables.
 
Resolution :
Yes, APC does manufacture an RJ45 Cat 5E rated coupler.
The part number is 47136WH.

This and other APC Cabling and Connectivity Solutions products such as Cat 5E, Cat 6 and Cat 6A cables, fiber optic cables, USB cables and adapters, multimedia cables, monitor cables...etc, can be found at: www.apccables.com.
Was this helpful?
What can we do to improve the information ?