Adding Additional Door Switch Sensors to a version 2 NetBotz appliance
Issue:
Adding Additional Door Switch Sensors to a version 2 NetBotz appliance
Product Line:
NetBotz
Environment:
NetBotz version 2
Cause:
Optional configurations
Resolution:
NetBotz sells additional door sensors that plug into the external sensor DIN ports. The DIN connector door sensor can be attached to any NetBotz monitoring appliance that supports DIN connector style sensors.
The NetBotz appliance can support as many door switch sensors as it has DIN connector ports.