Technical FAQs

Ask a Question

Audio Recording Capabilities on NetBotz 500

Issue:

Audio Recording Capabilities on NetBotz 500

Product Line:

NetBotz

Environment:

NetBotz 500 (NBWL0500)

Cause:

Audio recording capabilities.

Resolution:

 * Ability to capture audio when in alert condition
o Just like capturing pictures during alert condition
o Audio stream will be attached to each alert

* Ability to listen to current audio (listen real time)
o Link from camera view to stream current audio to default audio player

* Audio tracks are stored in .ogg format
o OggVorbis which is a royalty free MP3 type format
o Most MP3 players can also play .ogg files

* Data sizes:
o 1 second of audio is 4KB
o 1 minute of audio is 240KB
o 1 hour of audio is 14MB

Was this helpful?
What can we do to improve the information ?