Technical FAQs

Ask a Question

How to properly update an NetworkAIR FM NMC via XModem.

Issue:
How to properly update an NetworkAIR FM NMC via XModem
 
Product line:
FM
 
Environment:
Data Center Cooling
 
Cause:
 
Resolution:
NOTE: Start Update with the AOS and then the Application file. Every time you finish, you need to totally log out of HyperTerminal.

  • Open Hyper-Terminal Session /  set to 9600,8, None, 1, None
     
  • Hit enter key 2 times and input user name--apc and password--apc.
    

Note—this is the default high level user name and pass word; this may have been changed by site personnel.

    
  • From the control console enter: 3-System
       
  • 4-Tools

       

  • 6-File Transfer
       
  • 1-XMODEM
       
  • Respond YES
       
  • Select 4-Baud Rate 38400
       

  • Disconnect from Hyper Terminal, go to File, Properties and change port setting to 38400.

      

  • Click Apply, OK, then reconnect and press ENTER
        

 

  • Once connected the unit will start to Scroll CCC…  Showing connection is present
  • Click on Transfer, Send File…

 

      

  • 9. Click on Browse, locate file, and click Open. Set Protocol for Xmodem, click send.
         
 

 

  • File transfer will begin…
         

  • Once file transfer is complete, disconnect and exit hyper terminal session. Restart Hyper terminal session using the following port settings and check the control console for the proper AOS/Application files.
          



Was this helpful?
What can we do to improve the information ?