Technical FAQs

Ask a Question

Power Consumption of APC Rack Power Distribution Unit (PDU) / Automatic Transfer Switch (ATS) Products

 
 

 
Rack Power Distribution Unit (PDU) Type
 

Total Power Consumption (no outlets "ON")

 Wattage Draw Per "ON" Outlet

 Total Power Consumption (all outlets "ON" - assuming up to 24 outlets)


Metered (AP71XX, AP78XX)
 

N/A

N/A

approx. 5 watts



Metering By Outlet (MBO) (AP84XX)

 
N/A N/A approx. 11.5 watts


Metered (AP88XX)
 

N/A

N/A

5 watts


Switched (AP79XX)
 

approx. 5 watts

approx. 1 watt

approx. 29 watts


Switched (AP89XX)
 

5 watts

.5 watts

17 watts


Switched with Metering By Outlet (MBO) (AP86XX)
 

18 watts

.25 watts

24 watts


Rack Automatic Transfer Switch (ATS) Type
 

Total Power Consumption (no outlets "ON")  Wattage Draw Per "ON" Outlet  Total Power Consumption (all outlets "ON")


All models (AP77XX)
 

N/A

N/A

approx. 20 watts

All models (AP44XX N/A N/A < 20 watts

 

Note: These measurements don't include resistive losses due to current flow through the Rack PDU or Rack ATS meaning, they are only the fixed losses of the PDU or ATS associated with communications, measurements, and relay control.


 

Was this helpful?
What can we do to improve the information ?