Technical FAQs

Ask a Question

Can the APC NetShelter SV cabinet be disassembled to accommodate moving through a narrow doorway?

Issue: 
A customer needs instructions to disassemble a NetShelter SV cabinet. 

Product Line: 
NetShelter SV cabinets. 

Environment: 
All models, all serial numbers. 

Cause: 
The NetShelter SV cabinet needs to move through a narrow doorway. 

Resolution: 

We don't recommend disassembling cabinets because it voids the cabinet warrantee, but we understand that disassembly may be necessary to move the cabinet through a narrow doorway.
If you need to disassemble a NetShelter SV cabinet please use the assembly instructions for AR2400FP1 and follow them in reverse. AR2400FP1 is a NetShelter SV cabinet that ships flat packed (unassembled). 
Go to the APC website and search on AR2400FP1. Click on the Documentation tab and open the Installation Manual. 
 
Was this helpful?
What can we do to improve the information ?