Technical FAQs

Ask a Question

Can Data Center Expert post to a syslog server?

Issue:
DCE compatibility with syslog servers
 
Product Line:
StruxureWare Data Center Expert
 
Environment:
StruxureWare DCE 7.x
 
Cause:
A customer may want to direct system logs for Data Center Expert on a log server.
 
Resolution:
Data Center expert does not currently have the functionality to post to an external system log server.  You can however point the individual network management cards to a syslog server.  It is possible to perform a mass configuration through Data Center Expert.  http://www.schneider-electric.us/support//ye/en/faqs/content/?country=US&lang=EN&locale=en_US&id=FA316801
Here you can add a syslog server IP and port for your appliances.  For detailed information on each appliance, please contact the respective device support.
You can also individually configure NetBotz (3xx, 4xx, 5xx) devices to post directly to syslog under the "Log" option in NetBotz Advanced View.

 
Was this helpful?
What can we do to improve the information ?