Technical FAQs

Ask a Question

Are there instructions available showing how to install NetShelter seismic mounting brackets onto different floor types?

Issue: 
The NetShelter seismic mounting brackets need to be mounted to the floor. There are different floor types.

Product Line: 
NetShelter SX

Environment: 
All models, all serial numbers. 

Cause: 
The NetShelter seismic mounting brackets installation manuals only show mounting to the cabinet, not the floor. 

Resolution: 
Using the pallet bracket or AR7701 the NetShelter SX can be installed per IBC Low Seismic Area and Moderate Seismic Area onto a concrete slab, concrete fill over metal deck, raised composite floor concrete filled metal deck, and raised composite floor concrete slab.
Reference the IBC Seismic Calculations for NetShelter SX for instructions: http://www.apc.com/salestools/SNEL-8C7UQS/SNEL-8C7UQS_R6_EN.pdf 
An updated document can be loaded off the APC website of any NetShelter SX cabinet under the Documentation tab. 

Using AR7701A-S the NetShelter SX can be installed per OSHPD onto a concrete slab, and concrete fill over metal deck. 
Reference the OSHPD structural drawings for NetShelter SX for instructions: http://www.apc.com/salestools/JKUR-ATJL8V/JKUR-ATJL8V_R0_EN.pdf 
The AR7701A-S can also be installed to meet IBC High Seismic Area using these instructions: 
http://www.apc.com/salestools/SNEL-8C7UQS/SNEL-8C7UQS_R6_EN.pdf 


 
Was this helpful?
What can we do to improve the information ?