Technical FAQs

Ask a Question

Video: How to Shutdown your Symmetra PX 250-500 UPS

Issue:
Shutting down the Symmetra PX 250-500 UPS and transitioning critical load to maintenance bypass
 
Product line:
Symmetra PX 250-500
 
Environment:
All Product models, all serial numbers
 
Cause:
Shutdown Support 

Resolution:
Begin at the home screen of the UPS.
Select the wrench key at the lower left of the screen.
Select the 'Operation' button
Select 'System Shutdown'
 
Follow the step by step outline for shutting down the UPS. After each step is completed the option will be grayed out. Some steps will automatically be completed for you.

The following video demonstrates this procedure:
 
Was this helpful?
What can we do to improve the information ?