Technical FAQs

Ask a Question

What alarms can be automatically reset on a High Capacity Uniflair Unit

Issue:  
What alarms can be automatically reset on a High Capacity Uniflair Unit

Product line:
High capacity Models 4500/5000

Environment:  
All Serial Numbers 

Cause:  
Install  

Resolution:

The Automatic Reset allows the unit to clear the alarm and continue operation if the alarm condition is no longer present.

 

• High/Low Temperature Threshold Exceeded

• High/Low Humidity Threshold Exceeded

• Supply Air Temperature Threshold Exceeded

• High/Low Airflow

• Humidifier

• Smoke Detected

• Electric Heater Over Temperature

• Electronic Expansion Valve Error

• Low Pressure

• Circuit 1 Chilled Water High Temperature Threshold Exceeded

• Circuit 1 Chilled Water Temperature too High for Dehumidification

• Insufficient Chilled Water Flow

• Primary/Secondary Power Source Unavailable

• Dual Circuit Expansion Board Error Detected

• Digital 2/4/6 Input Abnormal

• External Sensor Threshold Exceeded

 

Was this helpful?
What can we do to improve the information ?