Technical FAQs

Ask a Question

Can I use the NetBotz leak rope sensors with the Network Air units?


NetBotz leak rope sensors can not be used with Network air units.

Product Line:



NetBotz version 3 and leak rope sensors NBES0308 and NBES0308


NetBotz leak rope sensors NBES0308 and NBES0308 have specific resistances that are expected by the NetBotz appliance.


The leak rope sensors AP9325 and AP9326 are designed specifically for the APC Network Air units they work with, You can not use these sensors on a NetBotz appliance nor can you use the NetBotz NBES0308 and NBES0308 rope leak sensors with APC's Air units.
Was this helpful?
What can we do to improve the information ?