Technical FAQs

Ask a Question

NetBotz v4.2 Web Client Does Not Run on IE8 or IE9 in Compatibility View

Issue:

The NetBotz version 4.2 Web Client does not run on Internet Explorer 8 or Internet Explorer 9 when displayed in Compatibility View.

Product Line:

NetBotz

Environment:

Microsoft Internet Explorer version 8.0
Microsoft Internet Explorer version 9.0
NetBotz version 4.2 Web Client

Cause:

It is a known issue that the NetBotz v4.2 Web Client does not function with the browser set to display websites in Compatibility View.

Resolution:

Change the Compatibility View Settings in the browser.

For more information about Compatibility View, see the following Microsoft article: http://blogs.msdn.com/b/askie/archive/2009/03/23/understanding-compatibility-modes-in-internet-explorer-8.aspx

This issue should be resolved with the release of 4.3
 
Was this helpful?
What can we do to improve the information ?