Technical FAQs
Technical FAQs
Issue:
Rack inlet high alarm
Product line:
Inrow
Environment:
Data Center Inrow
Cause:
Temp threshold is to low or sensor is in wrong place
Resolution:
Check threshold and check placement of sensor. Threshold should be at least 3 degrees above max normal temp and sensor should be place in the front of the server rack at least 6 inches from front of the server with blanking panels in any gaps in the rack