Technical FAQs

Ask a Question

Supported versions of software PowerChute Business Edition 9.0 can shutdown in APC Fast Recovery for Server Applications.

Issue:
What are the supported versions of software PowerChute Business Edition 9.0 can shutdown in APC Fast Recovery for Server Applications.

Product Line:
PowerChute Business Edition version 9.0

Environment:
All supported OS

Cause:
Informational

Solution:

These application versions are support in APC Fast Recovery for Server Applications

IIS: v6 / v7
Lotus Notes / Domino: v7 / v8
Microsoft SQL Server: 2000 / 2005 / 2008
Exchange Server: 2003 / 2007
Siebel: v4.0

Was this helpful?
What can we do to improve the information ?