Technical FAQs

Ask a Question

Video: Configure Back-UPS XS & RS LCD units for Full Time Display mode.

Issue:

The UPS display keeps turning off after several seconds. What are the steps to keep the display on all the time?


Product Line:

APC Back-UPS XS/RS LCD (Red Display)


Environment:

Normal Operation


Cause:

Display automatically turns off after several seconds.


Resolution:

The following video details the process to configure the Back-UPS XS & RS LCD units for Full Time Display mode.

Was this helpful?
What can we do to improve the information ?