Technical FAQs

Ask a Question

ISXC server constantly generate "FAILED TO TRANSMIT ALERT" events in the nbc.xml log

Issue:

InfraStruxure Central server constantly generate "FAILED TO TRANSMIT ALERT" events in the nbc.xml log.

Product Line:

InfraStruxure Central
StruxureWare Data Center Expert

Environment:

Any version

Cause:

A system that was once receiving web service events from your ISXC using the Web API has been disconnected from your LAN.

Resolution:

To resolve the issue, reconnect the system and unsubscribe or reboot your ISXC to clear the subscription.

Was this helpful?
What can we do to improve the information ?